What is a planar motor?A linear motor with two dimensions of freedoms
The planar motor is based on the principles of linear direct motors. The axis system consists of two main components.
The primary component is a rotor structure made of cast aluminum or stainless steel that includes permanent magnets, inductor elements and air nozzles.
The secondary component, the stator, consists of a stainless steel plate with a closely spaced grid of intersecting grooves on its surface. The grid spacing may be 1 or 3 mm. The stator grooves are coated with molded polymer (or polymer epoxy resin) and function as a gear structure, with sets of stator teeth and tooth gaps at right angles to each other in the X-Y plane.
|
|
The functional area of the rotors has polymer-molded gear teeth that interlock with the gear teeth of the stator. The surface of the rotor structure that faces the stator has nozzles connected to a compressed air feed. When the air supply is switched on and current flows in the system, the interplay between the air gap and the induction coils creates an air bearing of 15 ± 7 μm between the stator and the rotor, which allows the free movement of the rotor in the X and Y plane.
To achieve high power development and accuracy in movement and positioning, the hybrid stepper motors require faultless alignment of the rotor and stator. Incorrect alignment reduces operational efficiency. |
Requirements
Wear-free bearings, constant parameters, with smooth movement that is not impaired by slipping and sticking.
Simultaneous and independent motion for several rotors on the stator.
Construction of complicated axis systems, cross tables, main opening, XYZ-plane systems.
Work in all the planes of the available space – both overhead and in the horizontal plane.
Excellent dynamics via high acceleration and speed.
Operation as a step motor or as a regulated micro step servo motor and controller combination.
Maintenance-free, frictionless and wear-free.
Planar MotorThe planar motor offers a unique design that enables new motion
modes and protects the moving parts from losing force and "losing
their grip". All devices in the mobile component are Plug and Play!
Master-Slave Connection

Planar Motor Data
| Axis Name |
Controller |
Mission |
Y-Axis Master |
SOL-WHI-5/60E01 |
Obtain the Y position from the control unit |
X-Axis Master |
SOL-WHI-5/60E01 |
Obtain the X position from the control unit |
Y-Axis Slave |
SOL-WHI-5/60E05 |
Protect the Y-axis from rotation. The Y-axis Slave
obtains the position from the Y-axis Master via the
Master-Slave connection. This protects the planar
motor from losing force since it is stabilized and
controlled on the Y-axis. |
Maestro
| Axis Name |
Controller |
Mission |
Control Unit |
MAS-10012-1C |
The Maestro obtains the command position from the
PC and converts it to X- and Y-position coordinates. |
Motor Data
| Feature |
Specification |
| Type |
Servo planar motor (air bearing hybrid stepper motor) |
| Weight |
7 kg |
| Numbers of motors |
Three motors (1x X / 2x Y) |
| force per motor |
Maximum 40 N (at 3 A continuous current) |
| Special |
Y-motor in Master-Slave working mode (position control) to protect the motor against rotation |
| Air valve |
Onboard |
| Amplifier for addition application |
Onboard |
| Supply voltage |
48 VDC, 24 VDC |
| Communication |
CANopen |
| Inductive encoders |
Encoder system AMO, resolution 0.00025 mm |
| Encoder measurement system |
Stator of the motors |
The Challenge How to commutate a system when the measurement system is moving
| In contrast to other planar systems, the moving part of this planar motor includes the measurement mechanism. This mechanism makes the planar motor cheaper and provides
more options for different measurement systems.
No angle allowed The challenge of planar motor design is that it must be position-stabilized at
all times: The motor can only provide the full force if it is oriented correctly.
Even a small angle results in a huge loss of potential force. In the worst case scenario, the angle deviates so
much from the required position that the planar motor is not able to move and loses all commutation. |
|
The Elmo Solution
How the commutation works ?
| Movements |
Description |
 |
At start-up, the location and orientation of the planar
motor is unknown. The planar motor can only acquire
force if it is positioned correctly.
All feedbacks must be inactive and all the Y-axis SimplIQ Whistle
drives must move with the same speed relative to
the frame, |
 |
The planar motor moves to the outer frame in the "Stepper" mode (not using the feedback), to arrive at the correct starting position.
The twist is corrected and the SimplIQ-Whistle drives on the Y-axis are commutated. |
 |
The planar motor must move to a corner to define its second position. While moving, the motor must
continually verify that it is always correctly positioned with respect to the frame. |
 |
From the corner, the motor can commutate the X-axis. With all the axes commutating, the planar motor is able to
move in position mode and the Master-Slave protection is activated. |
How does the anti-angle work?
Because the communication is not sufficiently fast to handle the synchronization, Elmo
Motion Control recommends that both devices be set up in a Position-Follower
configuration. The YA[N]command for the SimplIQ-Whistle defines the behavior and
direction of the auxiliary position sensor signals. YA[4] is used to specify that the auxiliary
encoder pins shall be outputs, and shall repeat the pulses of the main position
incremental or analog sensors. This mode is used to enable other drives to follow,
without electrically overloading the main position sensor.
The situation is similar for the Slave. YA[4] = 2 sets up an auxiliary encoder entry that is
used as input for external quadrate incremental encoder signals. |
|
Program example: #@AUTOEXEC
YA[4]=2 // Set AUX feedback as quadrate incremental encoder command input.
FR[3]=1 // Set follower ratio to 100%
AG[2]=0 // Disable influence of analog input
RM=1 // Enable reference mode
UM=5 // Set position mode
MO=1 // Motor on
BG // Begin motion
Advantages of using the Maestro as a control unit
| Movements |
Description |
 |
The Maestro controls only the Master Axis for the planar motor.
Setting up the movement parameters. Both axes are controlled as vectors. At the beginning, after each movement, we want the motor to wait for new commands:
v1.attach()
v1.vsp=70000 // max velocity
v1.vse=0 //* end velocity*/ |
 |
Achieving point-to-point movement. Initially, we want the motor to start at 0 and move to a position in the field.
v1.line(70000, 100000) //go to position (7000,10000)
v1.bg //action! |
 |
Achieving more interesting motion. It is more useful to work as a vector from this location.
What we want:
Radius 50000,
Start angle 180°
3/4 turn=270°
v1.circle(50000, 180, 270) // create circle
v1.bg // start motion |
Important considerations
- Standard voltage is 48 V DC. It is possible to work with up to 85 V DC for high speed applications.
- Reduce the amount of cabling to greatly improve performance.
- Plug and Play functionality simplifies the motion system.
- Closed loop functionality provides very high resolution and better control.
- Smoother movement is possible because all the axes have one feedback system.
- Control at a low level is enabled: The Master-Slave control needs to be extremely fast and precise.
- Mass is important because all the devices are moving.
PASIM Direktantriebe GmbH was founded in 1991 by Dr. Günter Dreifke, based on the knowhow
of the Technical University of Ilmenau. This expertise, coupled with knowledgeable,
experienced staff and patented solutions is, to this day, the foundation and guarantee of
sound, steady technical and corporate development.
The core business of PASIM is the development, manufacture, distribution and servicing of the
company's air-mounted direct drives and systems. The advanced mechatronic products are
produced by the company's personnel in close cooperation with regional partners. The
company employs seventeen staff members. |
|
Why Elmo:
- Advanced motion and servo control
- Distributed networking
- High density coupled with high power
- High reliability
- High efficiency
- Easy to use: Reduction of complexity
- Compact Size
|