The Requirement: Compact, High Power Density Motion Control with Standard Communication and a Short Time-to-Market Solution in a Demanding Manufacturing Environment
Elmo's Solo Guitar digital servo drives are intelligent, high power and compact. This case study shows how one of our customers, a leading mobile robot manufacturer, implemented Elmo's Solo Guitar drives in a portable, heavy duty transport application. This case study will interest you if you require the following in your application:
- Implementing up to 5.4 kW of peak power using a servo drive the size of a cellular phone.
- Placing the unit in a very confined space where small size is a critical design consideration.
- Using products that can withstand demanding factory conditions and are compatible with both brush and brushless motors.
- Minimizing development time and reducing the number of system components in order to achieve a short time-to-market.
|
|
Machine Description
The mobile robot is an innovative, two-wheeled, autonomous vehicle designed for delivery of heavy components. A unique feature is the capability to follow a line along magnetic tape for path guidance. This allows the robot to adjust dynamically to changing surface paths and continue to operate without interference.
The mobile robot uses Elmo's proprietary Solo Guitar intelligence to follow the line and accordingly adapt device behavior. If there is a deviation, Elmo's Solo Guitar compensates by adjusting the steering, which is done without using a multi-axis control module. The mobile robot can be used for a variety of load transfer operations and is especially suited to the automotive, packaging, aerospace and medical sectors.
The mobile robot implements a “master-follower” concept. A master motor outputs (emulates) the encoder of the “following” axis. This allows the “following” motor to use the master motor’s feedback, both as a reference and a target. Additionally, the on-board intelligence monitors the input (I/O). These actions are performed relative to the master axis as the steering method.
The mobile robot incorporates two Solo Guitar servo drives from Elmo’s SimplIQ Line, one for each of the two wheels.
The mobile robot’s dimensions require compactness, which allows for strategic implementation onto the available floor space, where economy is always a concern. Its small footprint allows the customer to implement cost effective, reliable automation in a production line, and to better utilize human talent which saves both time and energy. |
|
Application Challenges
The manufacturer’s main aims for the mobile robot were:
- To achieve quick time-to-market with the smallest, most cost effective mobile robot on the market that can handle loads of 1 tonne (2,000 lbs+).
- To implement competent, cost effective wheel steering technology.
- To obtain the most efficient mobile robot possible, utilizing the least amount of battery power for continuous operation over shifts, which allows for less frequent charging.
- To utilize a minimal footprint servo drive, designed to be small enough to fit easily into the robot.
All components used in the mobile robot must withstand a continuous shift environment and perform reliably with off-the-shelf components for quick time-to-market.
The mobile robot was required to be highly reliable with an extended Mean Time Between Failures (MTBF) for all its different motion functions.
As the product incorporated an adaptive line sensing technique, the motion commands have to be delivered and received swiftly and accurately to provide precise motion in challenging and delicate operations (e.g., charge station, block detection, emergency stop, etc.)
The compact size of the robot required motion control products that could supply high power density within a small unit.
Battery drainage is the prime concern for robust autonomous vehicles in manufacturing environments. Too many oversized components located within the vehicle create inefficiencies resulting in the need to recharge batteries multiple times within a shift. With Elmo’s advanced unipolar switching technology, servo drives can efficiently run motors and not waste current on conventional control.
Moreover, autonomous vehicles have other components in the system that could be eliminated, enabling overall system cost reduction to the manufacturer for a longer lasting investment. This is achieved by reducing between-shift inefficiency and increasing production utilization by running the motors efficiently.
Elmo's Solution
The Solo Guitar digital drive was chosen for this application due to its compact size, power range and intelligence.
The Solo Guitar is very compact, measuring just 80 x 61 x 46.7 mm and weighing only 200 g. It has a peak output of 1.7 kW – 35 A at 24 V.
Two SOL-GUI-35/60s were chosen to be installed in the mobile robot.
The Solo Guitar is a member of Elmo’s SimplIQ Line, designed especially for applications where compact size, integrated intelligence and high power density efficiency matter the most.
|
Solo Guitar Servo Drive
80 x 46.7 x 61 mm
(3.15" x 1.84" x 2.4")
|
|
|
- Compact size, well within a 100 x 100 x 50 mm envelope.
- Integrated intelligence to monitor input and output states over CANopen or RS-232.
- Embedded programs to run a master-following routine within the drive and to accept emulated encoder signals that eliminate the need for a multi-axis motion controller and an oversized embedded CPU.
- A short time-to-market solution that can be utilized during site support scenarios where an off-the-shelf solution is required.
- Supports an ambient temperature up to 40 °C.
The two Solo Guitars were installed in a specially designed location within the vehicle near to the motors. The connector types and locations were chosen to optimize the robot’s production and minimize maintenance. Elmo’s application engineers worked with the design team on-site in order to ensure successful integration of the products and shorten the time-to-market.
The Solo Guitar drives already include the capability to perform sophisticated motion control loops for precise movement, feedback inputs, programming capabilities and communication support. Elmo's implementation of the standard CANopen communication allows the line following processor to communicate device states to the Elmo input logic. Excellent connectivity reduces time-to-market and eliminates the need for extra components.
Elmo’s proprietary Composer software is used to program the commands for the Solo Guitar, and this enables the robot to perform precise tasks that require rapid and accurate movement.
Solo Guitar drives are very reliable and can meet the strenuous demands of 24x7 manufacturing environments. |
|
Why Elmo:
- Compact drive with a connector mounting interface that allows for an immediate time-to-market.
- High power density, efficiency and intelligence within a small package.
- High reliability in demanding 24x7 factory automation environments.
- Dedicated support engineers to ensure successful implementation of solutions on site.
- Fast, precise and smooth motion control without the need for a full multi-axis controller or on-board PLC that drain battery power.
- Standard communication protocols.
|