Home Page
Search
 

Composer-servo motor drive tuning

Software for setup and operation motion control systems

Composer is a sophisticated suite of Windows-based software designed for setup and operation of motion control systems using SimplIQ digital servo drives. It also includes an auto-tune wizard for automated single axis servo-drive setup.

Designed specifically for the SimplIQ line of digital servo drives, the Composer will work with any brush or brushless servo motor.

The tuning function of Composer captures a signature of the mechanical system and implements an optimal control algorithm. This algorithm typically includes PID filter, notch filter (resonance elimination) and gain scheduling (automatic gain adaptation to the speed).
Elmo Composer, Drives and Servo Motors System
Composer also includes advanced diagnostic features, allowing the user to evaluate the tuning process with on screen scope traces.
We are now able to provide a Bode plot of a mechanical system and demonstrate, with the use of compound notch filtering techniques, how the Autotune anticipates resonant frequencies and successfully nullifies their effects.
This is the first commercially available auto tuning solution that goes beyond a marketing trick. Composer will improve the performance of every existing servo system, eliminating days, if not weeks of fine-tuning work that is typically the task of the design engineers.
Standard Features
  • Application and communication set up.
  • Automatic tuning of the current loop response, velocity response and position response.
  • Automatic tuning of the commutation.
  • Edit and create PVT and ECAM tables using the integrated table editor.
  • Write and debug single axis application programs.
  • Save parameters in the application's database.
  • Send commands to the controller.
  • Monitor motion parameters and status.
  • User-friendly diagnostic functions including advanced oscilloscope views.
  • Demonstrate the capabilities and features of all Elmo digital servos drive (on-line and off-line)
The following plots demonstrate the tuning feature:
Position Response

Velocity Step Response

System Requirments
  • Microsoft Windows 95/98/NT
  • 20M of hard drive space
  • CR ROM drive
  • RS232 port
  • CAN card for CAN Open applications (refer to the operating manaul for supported products)
Downloads: Composer Documentation SimplIQ Documentation