Search
 
 

Frequently Asked Questions

General

 

 

General

How do I close an analog position loop without a digital drive?

Use a linear analog feedback (a potentiometer for example) and connect it to the feedback input of the amplifier. Connect your position command to the reference input. Then convert the amplifier to Current Mode and adjust the gain for best position accuracy.

What is the difference between PWM and Direction control, and Step and Direction control?

PWM and Direction is a digital method of transferring analog information. It is mainly useful when optical isolation is required between the source of the command and the amplifier. Step and Direction is a position control method and it requires a position controller on top of the analog amplifier.

We have an existing design that uses a linear amplifier with a bipolar power supply. Can we use the same power supply for a PWM amplifier?

The PWM amplifier requires a unipolar power supply. This means that the bipolar power supply is wasted when used with a PWM drive. If you insist on using your bipolar supply with a PWM amplifier, pay special attention to the circuit common connection and common mode issues. You may be required to isolate your reference command.

Analog Brush Drives

What is preferred for better speed control:
a low-voltage tachgenerator or a high-voltage tachogenerator?
a low-inductance tachogenerator or a high-inductance tachogenerator?

Higher voltage and lower inductance is preferred for servo performance with a tachogenerator.

I have a voice coil motor that has only two leads (like a brush motor) but has no brushes. Should I use a brush or a brushless drive for this type of motor?

Despite the fact that the voice coil motor is a "brushless drive", you can use a standard brush drive with it.

I have a ±10V differential current command signal. How do I connect it to the VIO amplifier?

Refer to the Handling ±10V Command Reference application note.

I have a ±10V single ended current command signal. How do I connect it to the VIO Amplifier?

Refer to the Handling ±10V Command Reference application note.

Analog Brushless Drives

Can we drive a brushless motor that has an optical encoder only but no Hall sensors?

There are many optical encoders in the market that provide the "Hall sensor signal" through optical channels. If your encoder is one of these, just treat these outputs as if they are Hall sensors and connect them to what is defined in the amplifier literature as Hall inputs.

Can we control the speed of a brushless motor with Hall sensors only?

Yes you can. Elmo has achieved 200:1 speed regulation with Hall sensor speed control using inexpensive analog drives.

What is better: a trapezoidal or sinusoidal brushless drive?

A good trapezoidal drive is a less expensive drive and it will satisfy most applications, especially the point-to-point ones. The sinusoidal drive is more expensive and is required for better low speed smoothness.

What is better: an optical encoder or a Resolver?

The resolver withstands a harsh environment better but its R/D circuit is expensive and it is also bandwidth limited. The optical encoder is more fragile than the Resolver but it performs better for servo applications and is also less expensive.

I have a ±10V differential current command signal. How do I connect it to the PIC (or FLU) amplifier?

Refer to the Handling ±10V Command Reference application note.

I have a ±10V single ended current command signal. How do I connect it to the PIC (or FLU) amplifier?

Refer to the Handling ±10V Command Reference application note.

Digital Drives

Why do we want to use digital drives?

Although digital drives are more expensive, they are friendlier than analog ones and have excellent long-term stability. Also, their serviceability is far easier than analog drives.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

  Categories: