Develop, test and fine tune single axis motion
Used In:
- Application development stages
- Testing motion control hardware
- Tuning servo drivers
- Analyzing motion variables
Used In:
The G-MAS Axis Motion is built in to the Elmo Application Studio (EAS). It can manage and control single axis motions, one-by-one, located under the EtherCAT / CANopen fieldbus Network.
Most of the motion commands provided by the G-MAS Axis Motion tool are based on the PLCopen standard. A simple user interface and built-in recording facility enable a user to test and analyze servo axes as individual parts of G-MAS based motion control system.
Developing, testing and tuning each axis one-by-one is a necessary preparation step for servo system components in any multi-axis application.