Elmo increases machine throughput and accuracy to speed manufacturing
The Background
The company manufactures advanced machines for bonding solid-state light-emitting diodes (LEDs) that are used in a wide variety of applications.
The Challenge
As an innovator and high-volume producer, the company was interested in faster and more cost-effective ways to produce industry-leading LEDs and wanted to improve the speed and accuracy of its automated die-bonding machines.
Elmo was challenged to produce a motion control solution that would achieve
- 90-degree PTP motion in 40 msec
- Settling time to ±25 counts in 5 msec
The Solution
Elmo applied its solution of a direct-drive rotary motor (DDR) shaft connected to a rotational load controlled by Gold servo drives and powered by a dedicated Elmo power supply.
The Elmo solution included:
- 3-stage gain scheduling and acceleration feed-forward servo-loop functionality
- Software high-order filters for velocity and position control loops
- High-velocity position loop bandwidths
The Benefits
Elmo’s solution went far beyond the requirement, further reducing the motion profile to a mere 35 msecs.
With Elmo’s solution, the die-bonding machine was able to settle into a very low ±15 count position error in only 5 msecs.
Using Elmo Application Studio (EAS), several hours only were needed to successfully implement the solution.
Motion Profile results, settling into +-15 Cnt position error after 35mSec
(30mSec motion + 5mSec Settling time)
Motion Profile results, settling into +-15 Cnt position error after 35mSec (30mSec motion + 5mSec Settling time)
Elmo’s solution provided:
- Accelerated machine throughput resulting in more output in less time
- High power in a compact size to fit the limited machine space
- Fast and precise machine operation
- Advanced software functions for enhanced servo performance
- Power consumption of only 12 amps in the power supply and 18.45 amps in the motor, both well within requirements
- Fast and easy implementation process
Elmo’s solution for this die-bonding machine is the state-of-the-art in accurate and speedy motion control, saving the customer time and money in implementation and execution. With industry-leading Mean Time Between Failure (MTBF), Elmo products continue to perform reliably at the highest levels in the field.