Elmo demonstrates a new motion controller, an AC Platinum servo drive, and two dual-axis servo drives for low and high voltages in Hall A at Booth A536.
Petah Tikva, Israel – March 21, 2024 – Elmo Motion Control, a global technology leader in motion control solutions, is pleased to announce its participation at the AIMEX (Smart Factory & Automation World) exhibition at COEX in Seoul, Korea. The 34th International Factory Automation Expo will be held from March 27 to March 29. Elmo will have on display the Platinum line of servo drives, including the new Platinum Bassoon AC drive and the newly introduced Titanium Maestro controller, and two new dual-axis servo drives: Titanium Castanet and Titanium Harmonica 2 Axes.
“We are excited to display the latest leading motion control technology at AIMEX. This year will be a showstopper with several Elmo displays of the next generation of advanced motion performance, including advanced functional safety,” stated Louis Lee, Elmo APAC Sales Director.
Elmo will display its Platinum Line and the following new solutions at AIMEX Korea 2024:
- Titanium Maestro is a third–generation motion controller that meets the emerging challenges of machine builders that require top-notch performance, speed, accuracy, and increased robustness. This motion controller offers advanced real-time management capabilities for multi-axis machines. Embedded with cutting-edge computational Quad‑Core CPU and extensive memory, it enables a breakthrough cycle time of 100uSec for each axis. With the coupling of Artificial Intelligence (AI) capabilities, image processing, and advanced Python programming, the Titanium Maestro is in a league of its own.
- Platinum Bassoon is the first AC servo drive in the Platinum Line with full functional safety. This solution supports up to 10 Amps at 230 Volts and up to 3.25 kW of continuous power. The drive is compatible with brushless, DC brush, and linear motors, or voice coil.
- Titanium Solo Castanet is part of the next-generation dual-axis Functional Safety servo drive, based on GaN Power Switching Technology, for low DC voltage applications. This solution has up to 15 Amps at 100 Volts and 2.4 kW of continuous power, which is set to be released in 2024.
- Titanium Harmonica 2 Axes is part of the next-generation dual-axes Functional Safety servo drive with a fully featured motion controller and local intelligence. This solution has up to 10 Amps at 200 Volts and 5.6 kW of continuous power per axis, which is set to be released in 2024.
To schedule a one-on-one meeting at AIMEX Korea, please register here: https://www.lp.elmomc.com/events/automation-world-2024/