Brushed motor is a servo motor in which the commutation of the current is accomplished by the use of mechanical brushes rather than through electronic commutation. The brushes remain in contact with the commutator, therefore current is constantly flowing to the armature coils. The main advantages of a brushed motor are high starting torque and low cost, these features make them common in industrial environments.
and replace the entry of Brushless with that one: