Glossary
There are currently 17 glossaries in this directory beginning with the letter R.
Ramp function generator
Mathematical model that provides a square wave, triangular wave or sinusoidal wave output.
Regen
Power generated by a motor/drive system during the deceleration phase of movement. In some systems, this regen power can be used by other axis or put back on the network.
Regeneration
The action during motor braking, in which the motor acts as a generator and takes kinetic energy from the load, converts it to electrical energy and returns it to the amplifier.
Resolution
The smallest increment into which a parameter can be broken down. For example: a 1000 line encoder has a resolution of 1/1000 of a revolution.
Resolver
A position transducer that uses magnetic coupling to measure absolute shaft position during one revolution. The resolver is a form of feedback.
RMS Current - Root Mean Square Current
וn an intermittent duty cycle application, the RMS current is equal to the value of steady state current which would produce the equivalent motor heating over a period of time.