Glossary
There are currently 3 glossaries in this directory beginning with the letter J.
Jerk limitation
Limits the rate of acceleration change during the movement of an axis. Its purpose is to eliminate mechanical jerking when speed changes are made.
Jitter free synchronization
In a master/slave configuration, it refers to the slave drive matching the speed of the master at an acceleration/deceleration rate that provides to a smooth transition.