Glossary

All | A B C D E F G H I J K L M N O P Q R S T V W Z
There are currently 4 glossaries in this directory beginning with the letter V.
Velocity
The speed at which a motor or mechanical system runs.

Velocity loop
A servo control function that sums a velocity command signal with a speed feedback signal from a servo motor, and outputs the difference as a torque command signal.

Virtual master
An encoder signal created in the software of a motion control to allow synchronizing multiple servo systems. A typical machine may have several virtual master encoders.

VxWorks
VxWorks is a real-time operating systems that guarantees an absolutely deterministic response. It is increasingly used in motion control because of its real-time behavior, stability, operating time, and memory efficiency. (Dev. by Wind River Systems)