Automated Truss Manufacturing Powered by Elmo

…handling must be in place to reduce downtime. Auto-configuration: When new or replacement drives are installed, the control system must automatically commission the new node. The Solution Elmo’s Maestro was…

Elmo Rugged Drives Guide Space Missions

…broadly available and more affordable. When one such company sought to reduce costs by using commercial-off-the-shelf (COTS) components, they turned to Elmo Motion Control. Elmo’s ExtrIQ line of harsh environment…

The Gold Trombone network based high voltage servo drive

Gold Trombone

…fully featured motion controller and local intelligence. In conjunction with Elmo’s Gold Maestro, the ultimate distributed network motion controller, and the other members of Elmo’s Gold Line of intelligent servo…

Gold Twitter

Gold Twitter

…operate with single or dual power supplies. If separation between the main DC power source and a control supply is required, then a control supply (isolated from the Mains) is…

gold bee servo drive

Gold Bee

…from the Mains. The Gold Bee can operate with single or dual power supplies. If separation between the main DC power source and a control supply is required, then a…

The Gold Double Twitter is the world's most powerful miniature servo drive

Gold Double Twitter

…is isolated from the Mains. The Gold Double Twitter can operate with single or dual power supplies. If separation between the main DC power source and a control supply is…