High Power and Performance in Extreme Conditions for Radio-Controlled Robot
Superior motion control on the battlefield isn’t a perk—it can save lives. So, when an unmanned vehicle manufacturer developed a remote-controlled, all-terrain robot for harsh environment applications, they turned to Elmo’s Gold Bee servo drives for high-performance, reliable motion control tuned to navigate even the toughest environments. Read the story here.
Play AudioDistributed servo control for Semiconductor Wafer Inspection machine powered by Elmo
The high-volume production demands on an automatic testing machine for semiconductors, MEMS, and electronic boards required a compact, robust motion control solution
Play AudioMiniature Servo Drive Performs under Pressure in Deep Sea ROV Testing
When All Oceans, a British expert in underwater engineering, wanted to build a fly-out ROV which would operate in some of the deepest parts of the ocean, they turned to Elmo.
Play AudioHigh-power drives enable high precision force control for pick and place machine
A new Generation of Pick & Place machinery has demanded that in addition to producing fast throughput and very high accuracy, it would control with high precision the mounting force of the placed components.
Play AudioBoosting Performance of Turret Test Handler Machine
The turret test handler machine is used to perform tests identifying physical defects and determining the electrical integrity of the internal circuit of the semiconductor components.
Play AudioHigh Precision Gantry-based Dispensing Machine powered by Elmo
Innovative dispensing robot delivers outstanding speed, precision and flexibility for demanding applications.
Play AudioLaser Cutting Solutions at the Forefront of Technology
When an innovative laser equipment manufacturer sought to produce next-generation laser-cutting machine, Elmo’s servo drives and controller proved the best fit.
Play AudioPrecise Automated Semiconductor Testing Enabled by Elmo
A leading manufacturer of precision technologies for the semiconductor industry has turned to Elmo for building a smaller machine with better performance.
Play AudioRevolutionizing parking with an automated guided vehicle
An autonomous guided vehicle (AGV) needed high power in a small package for a safe, reliable, effective and space-saving parking.
Play AudioHollywood Captures Explosive Action with High-Power Servo Drives by Elmo
Elmo’s servo drives and software are helping cutting-edge movie cameras travel at explosive speed on a semi-autonomous, high-speed robotic dolly system.
Play AudioCutting-Edge Motion Control Accelerates Bottle Labeling
Elmo provides new leading industrial quality performance for labeling and capping machines with line speeds of over 60K labels per hour.
Play AudioSmooth, Precise Motion for a Heavy-Load Transport System
WFT upgraded its industrial transporter with Elmo’s Gold Drum servo drives, and gained high current over extended periods
Play AudioMastering the Motion Control Challenges Posed by Stress Test Stations
Stress tests often put a component under the stress of an entire product lifetime in a few days, and every aspect must be tightly controlled. When Heitec AG looked for precise motion control for its high-end testing stations for advanced products such as medical devices, it turned to Elmo’s Gold Whistle servo drives. Read why.
Play AudioHigh power-density drives help NASA dig up dirt in space
NASA developed a robot to mine dirt and rock in low-gravity, rugged conditions using Elmo drives to power its complex movement.
Play AudioIntelligent servo drives help lifting and conveying loads of varying weights
A leading manufacturer of AGV systems upgrades his latest model with Elmo’s advanced servo drives and solves a long-time operational problem.
Play AudioHigh-Power-Density Drives Run Mobile Robots in Smart Warehouse
The success of an e-commerce giant’s fully automated sorting facility hinged on low-profile mobile robots powered by Elmo’s compact, high-performance servo drives.
Play AudioHigh-speed, Omni-directional Unmanned Vehicle powered by Elmo
Unmanned vehicles have made quite an evolution throughout the years. Today, unmanned vehicles are tasked to maneuver through harsher terrains and environments.
Play AudioAutomated Medical Laboratories
Modern medical testing laboratories must automate their test procedures in order to lower costs and stay competitive.
Play AudioPowering Camera Positioning for High-Precision Print Inspection
If printing defects aren’t caught early on, they lead to lost time and wasted materials. Sophisticated machine-vision inspection systems can solve the problem, but they need the right motion control solution that can fit tight speed and size constraints. Read how leading print inspection company AVT solved the challenge.
Play AudioEnabling built-in flexibility and quality control in PCB production
Printed Circuit Boards (PCBs) are in our phones, laptops and almost every electronic device that we use. With the technology changing at breakneck speed, PCB manufacturers need more flexibility and better performance. But, with more flexibility comes greatly increased complexity. Here’s how a PCB printing machine manufacturer solved the motion control challenges, enabling greater flexibility and significantly higher throughput.
Play AudioAutomated Truss Manufacturing Powered by Elmo
A wide range of equipment is available to automate the truss manufacturing process.This project presented several challenges including greater scalability, additional features, and reduced cost
Play AudioBoost bottle capping and labeling efficiency with Elmo
A bottling company wanted to replace their mechanical cam with an electronic cam to improve efficiency without making major mechanical modifications.
Play AudioA Perfect Fit for a Bomb Disposal Robot by Elmo
A bomb disposal robot adapted for narrow spaces, such as in trains and buses, uses small, lightweight servo drives with built-in intelligence.
Play AudioThe Eco Car, Steer by Wire Technology and the Race to Save Energy
Some of the advantages of steer by wire technology are clearly apparent, as demonstrated in the Shell Eco-marathon, an energy saving competition.
Play AudioMotion Control at the Heart of Sophisticated Cardiac Imaging
For an advanced cardiac imaging system, the manufacturer needed a compact motion control solution with a fast serial communication channel.
Play AudioBuilding heavy-duty load capacity in a small mobile robot
Many robots can carry heavy loads, but not every robot can meet tight industrial requirements. When a leading robot manufacturer set out to build a small, cost-effective mobile robot that could handle loads of up to one ton, they needed a motion control solution with integrated intelligence and high-power-density. They found it with Elmo. Read more.
Play AudioElmo’s Solution for Diamond Laser Cutting
Elmo provides a comprehensive motion control solution tailored for the design and operation of diamond laser cutting systems.
Play AudioBoosting Performance of LED Semicon Die-Bonding Machine
The Semiconductor high-volume producer was interested in faster, more cost-effective ways to produce industry-leading LEDs.
Play AudioBoost Power and Agility of High-Mobility Robot with Elmo Drives
The Gold Whistle digital servo drive excels in handling both the extreme power requirements and the tight spaces of the high-performance Chaos robot.
Play AudioAdvanced motion control optimizes the C-Arm for better healthcare imaging
Elmo’s Gold Maestro network controller solution frees up computer processing to support improved C-Arm performance and better healthcare delivery.
Play AudioFlexible, Modular Laser Guided Vehicle Accelerates Time To Market with Integrated STO
A leading global supplier of innovative intralogistics and material handling solutions for warehouses turned to Elmo Motion Control to help it develop a flexible, modular laser guided vehicle (LGV) that would replace most of their shuttles on fixed rails.
Play AudioMotion control with high throughput for automatic test equipment
The high-volume production demands on an automatic testing machine for semiconductors, MEMS, and electronic boards required a compact, robust motion control solution
Play AudioSpeed up wafer testing by 30% with Elmo’s fast-settling servo drives
The right servo drive helped a semiconductor test-equipment manufacturer increase wafer testing speed while maintaining the highest quality and precision standards.
Play AudioAdvanced Driver Assistance Systems (ADAS) Powered by Elmo
Elmo’s servo drives are helping AB Dynamic build high-power, low-profile Advanced Driver Assistance Systems testing platforms
Play AudioPrecise Elmo Power for Robotic Neurosurgery
In neurosurgery, the difference between helping and harming a patient can come down to microns. That’s why Imperial College London researchers turned to Elmo.
Play AudioFighting Covid-19 with an automated lab testing system powered by Elmo
Rapid testing is key to fighting Covid-19. An automated testing system, powered by Elmo drives, helps labs speed up the pace.
Play AudioYarn Winder
The company for which this application solution was developed is one of the largest manufacturers of textile machinery.
Collaborative Robot
Elmo’s ultimate Motion Control solution is boosting the new design and answering the challenges of the first manufacturing floor Collaborative Robot Coworker developed by Siasun, a leading Chinese robotic company.
Highly Precise Movement for Clean Room Robot
A Semiconductor company specializing in automatic production for cleanrooms was building a robot for moving LCD panels.